Hi team,
Customer have some confusions on some parameters definition of UCC21530-q1:
1. How to define the CTI(comparative tracking index)? is that tested on the IC package materials?
2. The Channel to channel internal isolation voltage is 1850V, but the distance between these two channel is only 3.3mm. How to figure out the isolation voltage(1850V)? is it a tested value or a calculated value? whether the isolation voltage have some relationship with CTI? and what's the relationship?
Thanks!