Related to an earlier inquiry regarding the oscillation seen in the BQ25071, I have finally identified the issue.
When supplying the BQ25071 with output from a solar harvester, the load introduced when the BQ25071 turns on (VIN rises to 3.5 or above) results in the MPP reducing the current to maintain the voltage on the harvester output. Nonetheless, the LDO, specified to maintain 4.9 volts, is unable to maintain 4.9 volts when the voltage input drops. This results in an oscillation at the LDO and hence the TS divider. When the TS voltage falls out of range the device turns off. This results in oscillating load to the harvester.
This seems to occur when the battery voltage (Lithium iron phosphate) is below 2.9 volts. Everything works well above this voltage. Cannot understand this battery voltage impact on the charging circuit other than increased charging current at low voltage and hence, larger load for the harvester. I have disabled the Enable Iset function by leaving this open circuit high impedance. Is the USB500 standard 500 milliamps of input current?
Questions:
a) Is there an easy way of disabling the TS monitoring. I have followed the datasheet with 490/100 kohms for the divider; this does not work.
b) Can I use a stable voltage source elsewhere on the board and divider to bring 1 volt to TS (12.5-25 % of LDO) OR !!! is the threshold 12.5-25% of the instantaneous LDO voltage?
c) The TS threshold is 25milliseconds out of range. Can a large capacitor across the divider smooth the on-off waveform to lengthen the time in range until battery voltage rises?
d) If larger resistors are chosen for the TS divider might this, in combination with a parallel capacitor, keep the TS voltage in range?
Thanks for your assistance.
Jim