This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM3553: LM3553 driving 6.6V LED has high frequency noise

Part Number: LM3553


Hi support :

LM3553 driving Vf 3.3V Red LED is ok.

But I change Vf 3.3V Red LED to a new OSRAM GR PSLR31.13 LED.

The Vf of GR PSLR31.13 is about 6.6V.

When turn on the LED.

There is a high frequency noise.

Maybe the noise come from inductor.

And the light of LED seems to change a lot from the sensor reading.

The schematic is the same as the page 1 of the datasheet.

The only difference is the inductor is 3.3uH.

But the schematic is ok in Vf 3.3V LED.

If I change to Vf 6.6V LED.

Is there anything I need to change in schematic?

best regards

Only