Hi
Provide case details or comments: If SRN voltage is greater than VCC, indicating that a battery is the power source, the BQ24650 enters
low quiescent current (< 15 µA) SLEEP mode to minimize current drain from the battery.
VCC is set to 5.5V, battery voltage is 8V, SRN measures 8V, VFB=1.3V, at this time the battery is powered, and the battery power consumption is 70uA,but the SPEC is 15UA.
Thanks
Star