Since customer is suffering the output damaged of the UCC21530 issue during surge test (Worse case with 6KV at LINE to Nature), they modified the C_filter from 100pF to 1nF with R_filter=100R and increasing the dead-time a little from 1.2uS to 1.5uS(Working freq=20KHz). The damage issue is gone so far. However, customer wondering to know if these filter values are optimized and meet device's requirement or not? On the d/s, the recommended input filter cap is in range of the 10pF to 100pF. Is there any problem with 1nF?
application: 3 Level DC-AC Solar Inverter
Regards
Brian W