Hi,
According to datasheet, current limit is 2A~5A.
Base on equation, if I use Rlim=24.9kohm get 1.45A current limit.
My question is can I set current limit 1.45A of the e-fuse?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Jim,
The accuracy of current limit varies with process, voltage and temperature. The value of current limit from 2A-5A will have a tolerance of 15% and are quite accurate and recommended .
You can choose RILIM 24.9kohm to get current limit of 1.45A but it will have a tolerance of around 20-30% which may not be acceptable for your system.
Please refer this graph for more understanding:
Regards
Kunal Goel