This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS628502-Q1: UVLO Falling Threshold

Part Number: TPS628502-Q1

Hello,

My customer is asking if the UVLO falling voltage threshold can be changed to 4.5V (from 2.5V, TYP spec) by OTP setting in TPS628502-Q1?  They are currently using this device and prefer not to re-spin the board to achieve a higher UVLO falling threshold (by changing buck converter, or by adding an external reset IC, for example).

Thanks,
Alan