hello
what is the input / output max rang that we can use the part
we need :
9-36 input
24 - 29.5 output
we can't get i with the webench application
if the part can't get the rang please recommend a different one
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hello
what is the input / output max rang that we can use the part
we need :
9-36 input
24 - 29.5 output
we can't get i with the webench application
if the part can't get the rang please recommend a different one
Hi shraga,
Thank you for your interest in LM5122.
Are you talking about voltage or current?
The max input voltage is 65V, and min input voltage is 3V (4.5V for startup).
The max output voltage is 100V.
Thanks,
Yinsong
Hello Vinsog
1. please take a look o the schema that we sent you
it was design for 9-36v input 24 v out put
please check if we have a any mistake
Shraga6403.LM5122.pdf
Hello Yinsong
Let me ask you if we can take:
LM5122EVM-2PH board and change some parts so we can get the range that we need?
9-36v input
24 or 29.5 volt output ?
thank you in advance
Shraga
Hi Shraga,
Sorry for the delay.
Yes, the input/output voltage is ok and the EVM modification could be done.
Please note that it will enter bypass operation mode after Vin> Vout.
Thanks,
Yinsong
Dear Yinsong
What is the max output current that we can get with this EVM ?
We need 12A on the output at 29.5 Volt.
Thanks in advance
Shraga
Hi Shraga,
It really depends on the thermal performance of the FET, inductor, diode, etc, which is limited by the Vin min condition. Comparing your Vin min and Vout, they are very close to those of the original EVM. So the max load should be similar. That being said, it is possible that the EVM 7A full load is not pushed to its limit but I'm not sure about it.
Thanks,
Yinsong
Hello Yinsong
can we change some of the parts value so we can get 10A on the output of the EVM LM5122EVM-2PH for test ?
this EVM has too channels - what is the benefit of this way ?
Thank you in advance
Shraga
Hi Shraga,
Actually it's not really values that set the limit but the power FETs (you may need to change some values like the current limit but that is not a problem). Generally, better FET with lower Rdson, Coss, and Qg will allow higher power delivery. But for this case, as 7A isn't too far from 10A, I would just power it up and see if it works and if not, what is the bottleneck.
Thanks,
Yinsong
And to your second question, the two channel benefit is too handle higher load current.
Thanks,
Yinsong
Good morning
What is the maximum current that we can get with this option - two LM5122 on board
Where we can get a schema at Orcad format for LM5122EVM-2PH
Thank you in advance
Shraga
Hi Shraga,
As I said, it's 7A max nominal so 3.5A per phase, but it worth giving it a try with higher load before the modification. There are only Altium files because that's what was used to create the schematic and layout.
https://www.ti.com/lit/zip/snvr485
Thanks,
Yinsong