Hi,
I would like to ask you about how to use the BQ2002/F device.
(question 1)
Is it necessary to disconnect the supply voltage to this device once when connecting another battery and charging from the beginning after detecting the end of charging?
Or can the device remain powered and recharge with another battery?
(Question 2)
Regarding the end of PVD, the data sheet states that fast charging ends if VBAT is 2.5mV±2.5mV less than previously measured values.
At this time, I am worried whether a slight voltage fluctuation will cause a false detection.
Is PVD detection only judged by the voltage value?
Or is there a separate function that detects inside the device to prevent false positives?
Best regards,