Hello,
I have a question on setting up the EVM of LP87564Q1.
Is there a way to load the registers constantly with a value? After powering the device, the default voltages are 0.6V. Can these values be changed?
And if so, are there examples available, that show how can this be done?
Programming the device via I2C is not applicable, since the voltages for the CPU are generated by the LP87564Q1.
thanks & best regards,
Jens