This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HI TI expert,
We need a power device to meet the following requirements:
1. Typical VIN=12V
2. default VOUT=0.82V without programming
3.Vout can be adjusted on the flying
4.Iout max=15A
According the above requirements ,we found TPS544B20 looks proper but need confirmation.
Please help to confirm if it can meet our requirement ?
As long as the adjustment range on VOUT is within the +/- 10% available range for the TPS544B20, then yes.
If your application does not require digital telemetry, you could consider the TPS549B22
If you require a larger range of adjustment, you could consider the TPS546B24A
Thanks Peter for support.
1.TPS544B20 datsheet describes the adustment range is -20%~10%, how about your saying:VOUT is within the +/- 10% available range for the TPS544B20, then yes.
2.What is the advantage of TPS549B22 Vs TPS544B20
Yes, the VREF_TRIM function allows the output voltage to be adjusted from -20% (480mV) to +10% (660mV) but the thresholds for Power Good do not adjust with VREF_TRIM so adjusting the output voltage more than +/- 10% can trigger PGOOD to go low. That is why I would recommend the TPS544B20 only for applications where the output voltage adjustment range is +/- 10%
The TPS549B22 is a simpler device with fewer PMBus options than the TPS544B20 and internal D-CAP3 compensation instead of external compensation. It also uses a newer generation of Power FET, so it is generally more efficient than the TPS544B20, but the TPS544B20 offers output voltage, current, and temperature where the TPS549B22 does not offer telemetry.