Hi,
Hope you are doing good.
We are trying to run the simulation model of ucc28704 based on the webench provided report.
The output is falling to zero and the VDD pin is reading 100V which is way too high from the datasheet.
I am attaching the tina file and the webench report below
AUX_12V_rev1_1 - autosave 20-10-03 16_44 - autosave 21-01-06 17_12.TSC
Can you help us understand why is it behaving this way?
We are using the same board setup and the board is failing to give an output of 12V. it is stuck at 110mV.
Thank-you
Warm Regards
Harini Krishna