Hi Team,
The device stopped working when a pulse current of 3.4A.
I believe that the Current Protection Limit was activated.
What is the current limit value (min/typ/max) under these conditions?
[Conditions]
Vin=12V
Vout=5V
L=4.7uH
In the datasheet, when Vin=12V, Vout=1.05V, L=1.5uH, min3.5V/typ4.2V/max5.3V.
Are there any conditions for the detection time?(The pulse width of 3.4A is less than 1us.)
Best Regards,
Kenji