Part Number: LM74700-Q1
Other Parts Discussed in Thread: TPS25947, TPS2663
I would like to use the ORing solution shown in Figure 14 of TI document SLVAES2 (Six System Architectures with Robust Reverse Battery Protection Using an Ideal Diode Controller).
Referencing this figure, VIN1 in my application is 6-11V and VIN2 is 5-24V. I want VIN1 to be disconnected when VIN2 is present, but it looks like if VIN2=5V and VIN1=10V (for example) then the Q1 body diode will conduct even if U1 is disabled.
If this is correct then I can change to the topology shown in Figure 15, which I had avoided due to requiring extra board space and higher quiescent current.
Thanks for any feedback - Jason