Other Parts Discussed in Thread: TPS22976
Hi,
I have a separate low power always on microcontroller connected to TPS659037 PMIC via I2C. PMIC powers other chips: FPGA, DDR etc.
My FPGA requires 1.0V/0.85V instead of OTP default 1.15V and I would like to supply up to 9A from triple phase SMPS.
Is there a possibly to use PMIC avoiding the OTP EPC controlled power sequences and instead maunally implement them by using my microcontroller? Any limitations in this approach?
Basically, can I start the PMIC so that it does not provide any output voltages but has I2C registers accessible?
What do I have to do to avoid accidental OTP power sequence activation? Connect power on pin and some other configuration pins to gound/VCC?
Best regards,
Anton Samuel