Dear TI Forum
I am having trouble with the LM3401 Board.
It is working fine when <= 14.5V is applied.
When Voltage is around 15V the LED is flickering and above 15.5V the LED is stable but Power is 50%.
Red Probe = LED Voltage
Yellow Probe = LM3401 L,D, P-MOS connection point
Stable running <= 14.5V stable 10W LED output
>= 15V unstable conditions and half power LED 5W output
LED Cree 3.2V@2.4A
Capacitor: C5750X7R1E226M250KA TDK
Coil: SRP1770TA-220M BOURNS
Diode: SSB44 VISHAY
Mosfet: IRF7416TRPBF INTERNATIONAL RECTIFIER, also tried STS6PF30L
Also tried C302 100nF instead 1uF for noice reduction
Also tried L301 15uH instead of 22uH