We completely removed the DESAT blanking capacitor, but the voltage on the DESAT pin is still ramping and takes about 7uSec to reach 7V. We also removed the Schottky diode that's was in parallel with the Capacitor but it did not make a difference with the timing. Finally, we verified the capacitance to be <5pF and still no difference. Is this an inherent function of the device? We are also thinking of using a pull-up resistor to speed up the timing.