This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS22919: Enable voltage

Part Number: TPS22919

Hi.

The ON Pin Low Voltage Range is from 0 to 0.35 V in datasheet. Question is, if the maximum low voltage of the device that will enable/disable the load switch is 0.4 V, the load switch would be disabled or there is a risk that it will not be disable?

Thanks.