Hello,
I'm trying to use the LMG3410R050 as a high side power switch.
In essence, this is the equivalent circuit I'm trying to achieve:
I’m using the SPICE model provided in SNOM689A and the following circuit simulated in TI-TINA:
NOTE: Please, see attached the TINA simulation file (.TSC) and the LMG3410R050.TSM macro model
High Side Power Switch - Test 001.TSC
The problem is the simulation shows the output voltage in the load only goes from 0V to 10V and not to 270V (VBUS) as intended.
I will greatly appreciate if anyone can offer some insight in how to achieve the intended functionality.
Thanks in advance.
Regards,
Vicente Escaño