This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28704: PMP11600 Design Queries

Part Number: UCC28704
Other Parts Discussed in Thread: PMP11600

I need support for UCC28704 based PMP11600 design. In the design I don't see any provision for over voltage protection for SMPS.

Do you have any reference which will help to turn off device or supply at voltage above 275VAC or 300VAC.

  • Hi Shrikant,

    What you said over voltage protection is input voltage OVP , or output voltage OVP ?

    UCC28704 don't has input voltage OVP but has Output voltage OVP .  it detect the Vout through VS pin. OVP point is 115%Vout_reated .

    details setting of VS pin please find in datasheet page 10.

    Thanks.