Other Parts Discussed in Thread: TPS55288
hi,
I would like to know what is the maximum duty cycle the TPS61288 can operate?
thank you
Hen Lange
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Lange,
Isn't the Vout voltage a fixed voltage?
TPS61288 is a boost converter so it can't generate a Vout lower than Vin.
If you need to generate 8V from 16V Vin, the buck-boost converter TPS55288 fits for your application.
hi,
the Vout is changing according to the required operation. it is not lower then Vin. we have a power switch in case we need low voltage.
we need only a Boost, not Buck
is your PSpice model is enough accurate to simulate the transient response?
out load current is periodically (200 Hz) changing from 0 to 2A and back.
thank you
Hen