Other Parts Discussed in Thread: BQ2970
Hi,
Could you recommend proper protection IC for single cell?
Cell: LiFePO4, 1 cell
OVP: 3.7V~3.75V
battery operating range: 2V~3.65V
Required high-side protection.
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi David,
Our options for 1S protection ICs are either the BQ2970 or the BQ2980. The BQ2970 is a more cost effective solution with low side FETs. The BQ2980 features high side FETs and a sense resistor for more accurate protections. You can see the configurations available on the device configurations section of their datasheets.
It doesn't look like we have a configuration available with those specific thresholds. You will have to choose the closest device that we currently have available.