Hello everybody,
I use the bq25887 to charge two batteries pack separated.
I need to know the properties of the battery protection system but the chapter is empty.
Where is the chapter "8.3.10 Battery protection" of the datasheet ?
Thanks..
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello everybody,
I use the bq25887 to charge two batteries pack separated.
I need to know the properties of the battery protection system but the chapter is empty.
Where is the chapter "8.3.10 Battery protection" of the datasheet ?
Thanks..
Hi Sebastien,
Sorry about that. The pdf generation for this datasheet had an issue. Below is what it should say.
8.3.10 Battery Protection
8.3.10.1 Battery Over-Voltage Protection (BATOVP)
The battery over-voltage limit is clamped at 4% above the battery cell voltage while charging. When battery over-voltage occurs, the charger device immediately disables charge. The fault register BATOVP_STAT bit goes high and an INT pulse is asserted to signal the host. The battery regulation voltage can be changed by JEITA_VSET bits and battery temperature, but BATOVP set point will not change.
8.3.10.2 Battery Over-Discharge Protection
When the battery is discharged below VBAT_SHORT_HYS, the BATFET is turned off to protect battery from overdischarge. To recover from over-discharge, an input source is required at VBUS. When an input source is plugged in, the BATFET turns on. The battery is charged with IBAT_SHORT current when the VBAT < VBAT_SHORT, or pre-charge current as set in IPRECHG registers when the battery voltage is between VBAT_SHORT and VBAT_LOWV.
Regards,
Jeff