Other Parts Discussed in Thread: UCC39002
Hi,
Could someone please confirm which exact, orderable part numbers from the UCC2900x and UCC3900x series of parts include, and do not include the start-up logic functionality described on pg. 9 of the datasheet?
Do you offer any versions of this part in a VSSOP package which does NOT have the startup logic function?
I'm confused because of two reasons. First, the datasheet contradicts itself and says that UCC29002 both includes the start-up logic, and then in the same paragraph also states that the UCC29002 does NOT include the start-up logic! And second, on slide 25 of "Load share control using the UCC29002" powerpoint presentation, the distinction is that UCC29002/1 does NOT include startup logic, the UCC29002 DOES include startup logic, and there's no mention of UCC39002.
Thank you!!
-Dom