Part Number: LM53625-Q1
Dear Sir/Ms.
The attachment is the circuit diagram of my customer. He asked if the input voltage is greater than 36V, will the output voltage become something? Is it a short circuit or is it greater than 6V? The customer also asked if the output voltage can be changed to 3.3V? Or can you recommend a more suitable solution?
Best Regards,
Kami Huang