Other Parts Discussed in Thread: BQ27531-G1,
Hello,
We're using the charger bq24192 together with the fuel gauge bq27531-G1 in a product.
The question is about the case when an adaptor is connected (VBUS=5,1V) and a charging cycle has just been terminated sucessfully. In case it matters, we have programmed the charging voltage to 4,05V and termination occurs when charging current drops below 120 mA.
Until recently, we were expecting for this case:
- Charging stops
- VSYS stays at ~4,05V and is being powered from adaptor
However, we have seen that rather this happens:
- Charging stops
- VSYS stays at ~4,05V and is being powered from battery
- After a while (~30 minutes), charging starts again
We have verified that Dynamic Power Management ist NOT active (the bit is not set and the adaptor is sufficently strong).
Is it expected behavior that the battery is discharged when an adaptor is connected? We observe an endless charge-discharge-cycle.
Can we influence if VSYS is being powered from battery or from adaptor? It would actually be great, if the host could configure this.
Thanks you in advance, best regards,
Nils