Other Parts Discussed in Thread: UC1825, UC1823
Hi!
Can I use the spice model of UC1825 to perform analysis to a design that is using a UC1823A-SP?
The only difference between UC1823 and UC1825 is the max duty cycle limit. Is the UC1825 spice model limited to 50%? If so, what needs to be changed to increase the maximum duty cycle limit to 90%?
Thanks!
--Luis