This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM60430: lm60430

Part Number: LM60430

Hi,

We are planning to use LM60430 in our design to convert 8-36V wide input voltage to 3.3V. We have two different BOM configuration, out of which in one configuration, the current requirement will be less than 3A. But n other one the requirement will be around 5A. So I am just wondering whether I can use two LM60430 in my design and short the output of both in parallel for better current capability.

So that in first configuration, I can mount only one regulator and in second I can mount both regulators to support higher current requirement.

Please suggest whether I can use two regulators in parallel or will there be any issues if I use two regulators in parallel?

Regards,
Shafeeq