Hi,
In our application it can happen that a voltage of 12 V (supplied by an external source) is present at the output of the TPS82130.VOUT (it is not guaranteed that the input voltage TPS82130.VIN is always present). Under normal operating conditions, the TPS82130 is used to generate a voltage in the range of 0.9V and 3.3V (TPS82130.VIN = 12V, voltage tracking function).
To protect the TPS82130 (and the supply voltage network at TPS82130.VIN) from the possible 12V voltage at TPS82130.VOUT, we want to connect a Schottky diode directly to TPS82130.VOUT and tap the feedback voltage TPS82130.FB after this diode. We know that the diode will reduce efficiency, but this is acceptable.
Is there anything against this solution or is there a better solution for this problem?
Is there an alternative DC/DC converter with true reverse current protection, an input voltage of 12V, an output voltage range of 0.9V to 3.3V and the tolencee to an externally supplied voltage at the output of >= 12V?
Thanks for your help!