Other Parts Discussed in Thread: TMDSEVM437X
Dear
I need to calculate the pullup resistor of a I2C bus connecting TPS65218D0 and other IC
What is the input capacitance of the SDA, SCL input of the TPS65218D0 PMIC?
Regards,
Sébastien
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear
I need to calculate the pullup resistor of a I2C bus connecting TPS65218D0 and other IC
What is the input capacitance of the SDA, SCL input of the TPS65218D0 PMIC?
Regards,
Sébastien
Sébastien,
I apologize, but if this value is not in the TPS65218D0 datasheet then I will not be able to locate this information in a reasonable amount of time.
Please refer to the TMDSEVM437X for the recommended I2C pull-up resistor value, which is 2.2kOhms for SCL and SDA when pulled up to 3.3V for I2C communication. There is ID EEPROM and a camera expansion header that also connect to I2C0 bus.
Dear,
I am surprise about this answer. on I2C bus, Bus capacitor is a key parameter to calculate the pull up. All IC I use indicate this Cin value on its spec.
Regards
Sebastien
Sebastien,
I understand. I am as surprised as you are that the Cin value is not specified. I have asked if any data is available in an internal repository or if the Cin value can be determined by running a simulation, but I cannot guarantee that this will happen for a device that was originally designed prior to 2014.
Based on the information available to me, here are the options that are available to continue debugging the issue:
1. Decrease the RPU (pull-up resistor) resistance value
2. Modify the software to use Standard-Mode (100kHz)
Below are the simulated + estimated parasitic values for Cin on I2C lines: