Other Parts Discussed in Thread: LM5068, , UCC28730-Q1, UCC28730, UCC2897A
Hi Team,
Is there AEC-Q version of below devices?
LM5026MTX/NOPB
LM5068MM-2/NOPB
Thank you.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team,
Is there AEC-Q version of below devices?
LM5026MTX/NOPB
LM5068MM-2/NOPB
Thank you.
Hi,
No, LM5026 and LM5068 do not have Q1 version.
If you can use other devices of TI, and like to know if they have Q1, you can search with -Q1, for example, UCC28730, its AEC Q version is UCC28730-Q1. If your search return say not find, it means no such version for that device.
Could you recommend using any other AEC-Q IC to replace LM5026(active-clamp forward) and M5068 (hotswap and current limit) ?
BR,
Gary
Hi,
TI does not have a device with active-clamp forward on AEC-Q grade. If only temperature grade is considered, you can consider UCC2897A, which temperature range is -55C to 150C. You can click the below link and click Active Clamp to find if there is a device that can be used.
Also, TI does not have a device with AEC-Q grade close to LM5068. Actually there are only three Q1 graded devices for hot swap. You can review the list on this link to decide if any can be used.