This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61391EVM-058: Power management forum

Part Number: TPS61391EVM-058


Hi

For the above evaluation board, understood the board is able to step up voltage to 30~85V

1. it it possible to create step up voltage +/-30 v~ +/- 85v? What I need to do to achieve it?

2. Can the +/-30 v~ +/- 85v be adjustable for example to +/-70v?