Other Parts Discussed in Thread: CSD
Dear Forum,
I am little bit confused when calculating PCB heatsink surface-ambent Rth.
In the device datasheet a reference given: (2) Device mounted on FR4 material with 1 inch2 (6.45 cm2), 2 oz. (0.071 mm thick) Cu.
Yielding Rthja = 50 C/W (neglecting Rthjc which is very small).
However, it is not menitoned whether this is 1 inch2 area achieved by sum of TOP/BOTT or by single layer or 1 inch2 exposed onto both side.
According to AN-2020 application note: for double side heatsink: Areq=155/(2*Rthsa) - >1,55 inch2 would needed for 50C/W.
AN-2020 also states A=155/(2*Rthsa) formula takes account to radiation as well, by calcualting a (radiation) modified coefficient heat of transfer parameter (by choosen to 10 W/mK)
For 1 inch2: Rthsa=(1/h)*/A=(1/10 W/m²K)/0,000645m²=155 ⁰C/W.
Thanks and regards,
Joseph