Other Parts Discussed in Thread: LM61440
I'm trying to create BUCK regulator using TI LM61440 with the next input
Input voltage 9 -16V
Case 1:
output : 5V@2A
At 2MHz switching frequency it works
When I'm trying to reduce the switching frequency from 2,2MHz to 1,2 MHz ( or around) WEBENCH generates error message "Unstable design"
output 5V@1A
switching frequency 2MHz
WEBENCH generates error message "Unstable design"
Question : Is it LM61440 Model trouble or it reflect the actual behaviour?