Other Parts Discussed in Thread: TPS2116
Hi,
I use the LM60430 to do a step down converter : 12V to 5V / 2A.
I need to add a super capacitor on the 5V power supply.
I would like to know if I have to add a serial diode between the SW ouput of the LM60430 and the super capacitor, for example when there is not a supply on the VIN input :
If the ouput impedance is high a serial diode is not required,
But, if the output of the LM60430 is shunted to GND, I have to add a serial diode in order to avoid to discharge the super capacitor.
Please can you give me the output impedance value of the LM60430 when it is not supplied
Thanks,
Jerome