Other Parts Discussed in Thread: TPS23880, , , TPS2378
We're looking to integrate POE++ into our device, but are need some expertise on how LLDP fits in the equation. Based on what I've read about POE++, when we plug into a POE port, the PSE applies a small DC voltage between the wire pairs and measures the received current. This is done at a regular interval to ensure the PD is still there. Then once were discovered, the PSE initiates a classification test where we indicate what power we need (based on the resistor values we choose for the PD controller). The PSE will then indicate what it can allocate to us and demote us if necessary. There are 3 outputs on the PD controller that will tell us what power we were allocated. For our application, if the allocation is 40W+ we can then use that to turn on the DC-DC controller and boot our SOM. From there the SOM can begin negotiating over LLDP?
The LLDP part is not clear to me. Are there switches that solely rely on LLDP to negotiate power? Or is this hardware negotiation standard on every 802.3bt switch? Do we even need LLDP at all?
Thanks!