I want to know the minimum SW frequency and maximum SW frequency at 5V input. A SW frequency graph with 5V input is also required.
reference
SWITCHING FREQUENCY
ƒSW Switching frequency at VIN = 3 V Min 0.75 Typ 1.2 Max1.5 MHz
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I want to know the minimum SW frequency and maximum SW frequency at 5V input. A SW frequency graph with 5V input is also required.
reference
SWITCHING FREQUENCY
ƒSW Switching frequency at VIN = 3 V Min 0.75 Typ 1.2 Max1.5 MHz
Hi Kazuo,
We don't have the accurate SW frequency data when VIN is 5V. Besides, this parameter doesn't vary a lot comparing to VIN=3V.
BR,
Robin