Hello,
I am looking for a 24V @ approx 2A POE flyback buck solution for the 23730. I found a 50W TI 5V@10A, 12V@5A and love to see a 24V@2.5A design.
Are there any 24V POE class 3 reference designs in your quiver?
Bruce
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I am looking for a 24V @ approx 2A POE flyback buck solution for the 23730. I found a 50W TI 5V@10A, 12V@5A and love to see a 24V@2.5A design.
Are there any 24V POE class 3 reference designs in your quiver?
Bruce
Hello Bruce,
Unfortunately we do not have any designs at this output voltage and power level. My suggestion would be to use one of our reference designs that are 24V output and then modify it for 2A (instead of 3). This would involve changing the transformer, but since the turns ratios should be close, the work of changing it would be minimal versus designing your own DCDC.
We have an ACF and a flyback 24V/3A design. Also i understand it is not with the TPS23730, but the TPS23730 could be used in place of the PD and PWM controller.
If this post answers your question, please indicate so by marking this thread as resolved. Thank you.
Regards,
Michael P.
Applications Engineer
Texas Instruments