This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC27284: Mass production time of UCC27284

Part Number: UCC27284
Other Parts Discussed in Thread: UCC27282

Hi,

I'd like to know the mass production time of UCC27284.

And what is the difference between UCC27284 and UCC27282.

Thanks.

  • Hello Eric, 

    The main difference is that UCC27282 has interlock and UCC27284 does not.

    As for MP date, please reach out to local sales office for estimated timeline.

    Regards,

    -Mamadou

  • Hi,Mamadou

    Thanks for reply.

    If the main difference between UCC27284 and UCC27282 is just interlock,

     the significance of UCC27284‘s launch seems not so necessary.

    What are the focuses of these two products and which one should I choose for servo control.

    Regards

    Eric

  • Hello Eric,

    I work with Mamadou supporting these driver devices.

    For servo motor control, I assume the power train will be a half bridge. If the driver is driving a half bridge MOSFET configuration you normally do not want the low side and high side FET's on at the same time. In that case you are better off with the UCC27282 since it will prevent MOSFET cross conduction.

    For the target markets in general: The UCC27282 is targeting half bridge based power converters and motor drives (various configurations). The UCC27284  allow use in topologies that require both drivers to be on at the same time which include synchronous rectifiers and some power topologies such as two switch forward converters.

    Confirm if this addresses your questions, or you can post additional questions on this thread.

    Regards,