This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS63050: Start up Voltage

Part Number: TPS63050
Other Parts Discussed in Thread: TPS63805

Hello,

I had a question about the start up voltage of TPS63050. This device has a 1.7V UVLO, but it's input voltage range is 2.5 to 5.5V, EN also has a fairly low ogic H voltage(1.2V). 

I'm wondering what's the status when the input voltage is between 1.7 to 2.5V which is higher than 1.7V UVLO, but lower than required input voltage. thanks.