Hi
The customer was using the TPS61097A-33 for remote control.
TPS61097A Schematic : There is no problem with the boost action.
Input Voltage(VBAT) : 3V(AA*2)
Output Voltage : 3.3V
LED 1ea : 2mA
We designed to add Voltage detector IC to turn on and off due to specification changes.
Additional Voltage detector Schematic : Boost does not work
- Input voltage(VBAT) 1.7V or less Cut-off
However, the Vout voltage of the TPS61097A is not 3.3V (BOOST up is not possible) and the Vin voltage is output to Vout as it is.
Competitor IM8132S has no problem with BOOST UP operation.
Please check the schematic for problems..
Schematic Attachment :
PCB Layout :