Other Parts Discussed in Thread: CSD19534Q5A, CSD18563Q5A
Hello,
I have an issue with a 35-50V input 12, 18, 24 V selectable output buck converter designed using the LM5117 and the TI Webench for 10A output.
The issue is that when I apply even a small load e.g. 40ohm at 18V, the output voltage goes into a sawtooth. I think what is occurring is that the LM5117 is going into current limiting of some kind as I see a ramp at the same frequency on the SS pin. I have tried tying the RES pin to VCC, the performance gets better but the output voltage is still in a sawtooth waveform.
Below is my schematic and PCB design. I have a ideal diode circuit using the LM5050 on the output however I don't believe this is what's causing the issue.
I have replaced the 1uF capacitor on the CSG, CS pins with a 560pF and have a 10nF capacitor on the SS pin rather than a 47nF. FETs are IPB042N10N3GATMA1. Currently the external voltage regulator U2 and the divider R10,R11 are unpopulated (as I was concerned with the LM5117 overheating however in practice this was not an issue).
Below are scope pictures of the output voltage, voltage at SS, VCC and waveform at the drain of Q2 along with a close up of the switching part of that waveform.
OUTPUT
SS
VCC
DRAIN OF Q2 (SW)
Any help would be highly appreciated.
Thanks in advance!