Other Parts Discussed in Thread: TPS25200
Hello,
I noticed that despite that in the datasheet it is specified that the soft start pin is getting discharged with 5k if the device is disabled, I did not observe this on our circuit. The SS capacitor is quite large in our case (4u7), but the capacitor should be well discharged after about 50ms (+10ms EN latency). However, it discharges much slower in our case, so we need to add some external parts (a Schottky diode to EN with a 10k pull-down helps) to discharge it during a reset event.
Is this a known issue of this device?
Thank you for your answer!