According to the data sheet, TPS546D24A has AVS feature, but it doesn’t support AVSBUS, which is described in 7.6.9 (19h) capability read only register bit2 (default 0). I just found a few words in the datasheet, and haven’t found any further information in Ti website. Could you help to provide some documents about AVS in TPS546D24A?
TPS546D24A supports PMBUS1.3.1, AVSBUS is one of the features of PMBUS1.3.1, which defines standard commands for AVS. What does it mean TPS546D24Adoesn’t support AVSBUS, anything special for AVS in TPS546D24A?