I need a little help understanding how to determine the minimum amount of output capacitance for the TPS548A20. The data sheet indicates the minimum capacitance should have the LC pole close to the zero frequency. The design spreadsheet I found a link to on another forum post sets the minimum capacitance based on the LC pole < Fsw/30.
With a design for Vin = 12V, Vout = 5V @ 2A, Fsw = 1 MHz, Webench selected 33uF +22uF output caps with L = 6.8 uH. However, the calculated min output capacitance Webench provides says the design needs 103.47 uF min output capacitance. The selected caps don't meet this recommendation.
If I use the data sheet equation with fz = 12 kHz (for Fsw = 1 MHz), Cout min = 27 uF (webench selected caps look good for this)
If I use the data sheet equation with fz = 6 kHz (for Mode pin set for slower RC time constant), Cout min = 103.4 uF. This must be what Webench calculated but didn't follow when making the cap selection.
If I use design spreadsheet, Cout min = 3.35 uF. Seems too low to me. Spreadsheet also has Cout max recommendation: Fcl < Fsw/100, which works out to 37 uF in my case. The spreadsheet includes a comment that Cout can be above this needs but to be checked for stability.
I'm tempted to stay with the Webench selected values, but some clarification as to the best approach would be helpful.
Another comment about the Webench results. I found with different switching frequencies and inductors, that the calculated minimum output cap the Webench reports sometimes uses the faster injected ripple RC while other times uses the slower RC times constant to determine Fz. The schematic for the Mode pin doesn't change. It's not clear what criteria Webench is using for selecting the RC zero frequency.