Hi,
I would like to ask you about the UCC2897A device.
(question 1)
If I don't use the overvoltage protection function (LINEOV), can I set the LINEOV pin to GND?
(Question 2)
The data sheet shows the maximum duty under certain conditions (see figure below), but what is the maximum duty for this device in practice?
Under the conditions of RON = 87kΩ, ROFF = 54kΩ, and RDEL = 10kΩ, I have confirmed that the board I made can output up to about 77% ON Duty.
(Question 3)
The data sheet states that the external sync frequency should be set higher than the free-running frequency.
Is the following setting possible?
external sync frequency x 0.9 > free-running frequency
Best regards,