Other Parts Discussed in Thread: LMR33630
Hello team,
My customer uses LM2576 with an external protection circuit at /ON/OFF pin.
In the system, the /ON/OFF pin slowly rises in approx. 80ms.
Please find the internal link here for the waveform. (Please connect to VPN for download).
Do you think the slow input rising should be OK? What is the input type of the /ON/OFF pin (CMOS/BJT)?
I'm asking because if it is CMOS input, I guess the output can be unstable.
Regards,
Itoh