Hey team,
One of my customers had a slight design change request from their end customer and are looking for a way to disable the LEDs during a somewhat unique event. To give some more detail there are two use cases:
- Normal operation using a type-C cable. Chg/Dsg occurs normally and the user can see the SoC when a PB event occurs
- When the product is inserted into an device using the contacts on the top of the housing bypassing the type-C but using PD protocol. Whenever the product is inserted into a device, it will be discharging and powering that device – charging will never occur. When the product is seated in the device and a double tap/PB event occurs (more or less an on switch), the LEDs will light up and there will be light leakage. This is the issue. When the product is in the device, the PB event can still occur and illuminate the LEDs.
Their main ask is if there's a condition or setting that cane be changed within the BMS to disable the LEDs while it is connected to said device. The customer identified that it appears you can send the SMBus cmd to disable the PB but then there is no way to enable it once the product is disconnected from the device.
Thanks and let me know if you need more info!