This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS6594-Q1: Voltage on OVPGDRV

Part Number: TPS6594-Q1


Dear TI E2E Community,

I'm looking for more detailed information regarding output voltage on pin OVPGDRV pin which is used to controll the pass through MOSFET which is supplying the VCCA pin.

I see that there is internal charge pump times 3, so can we expect that the voltage in OVPGDRV is approx 10 V? According to the Recommended operating conditio R1.2 this pin is typical 11.5V.

What is expected voltage on the pin OVPGDRV under normal operating condition?

 

Thank you in advance for all your coments.


Tomasz