Other Parts Discussed in Thread: DRV8847, BQ24650, BQ25798
We designed in the LTC4162-SAD in a remote monitoring application as it was dedicated to lead acid which is needed for temp performance. We later found the bq25672. The TI part appears to do what the LTC will not do and that is regulate the load side of the charger to less than 18V so as to protect our TI DRV8847 motor driver which has a max voltage of 18V. The LTC part's power path is passed straight through to the load which could be close to 24V in a solar charger application. If I read the TI data sheet correctly the TI part would buck down the solar open circuit voltage to a setpoint less than 18V. This also protects our application if there is a battery failure in that the solar input could then power the load with a regulated voltage.
Second issue is chemistry. The bq25672/692 claim to be LiPO, LiFePO4 chargers. Can they be programmed to charge a 12V 1.3Ahr AGM battery?
And are these assumptions about the TI part correct?
Thank you for your help
Charlie Jenkins
Former Ti FAE.